Vacuum Components

All press releases around our product range "vacuum components" are listed here.
The main emphasis is on suction pads, vacuum generators, switches, complete systems and special costumer solutions. In addition to short press releases, this area contains detailed user reports and technical articles.

  • 10.10.2011
    700 Pages on Vacuum Components and Much More

    Schmalz presents the greatest variety of vacuum components the market has to offer in its new Vacuum Components Catalog 2012/2013.

  • 15.06.2011
    Turning Two into One: Safely Separating Double Blanks

    When automatically feeding raw sheets, sheet metal parts, blanks and other flat workpieces into forming machines, it is important to separate components and ensure that they are fed in individually to prevent damage to the machines. In conjunction with commercially available sensors, the double-blank detection unit DBD from vacuum technology specialist J. Schmalz does just that – precisely and reliably.

  • 10.05.2011
    Configured in no time

    Vacuum technology specialist J. Schmalz presents the first modular system for fast and easy setup of vacuum end effectors for the packaging industry

  • 31.03.2011
    A Knack for Sweets

    Truffles, cherries, balls or hearts – automated moving and sorting of chocolates must be delicate. To allow for dynamic handling of chocolates in various shapes, vacuum technology specialist J. Schmalz GmbH has added the SPG suction pad for chocolates to its range of products.

  • 24.01.2011
    Stronger, Sturdier, Smarter.

    X-Pump, the new generation of vacuum generators with integrated IO-Link technology optimizes robot-assisted handling of sheet metal parts.

  • 22.10.2010
    SAXM – New Vacuum Suction Pads for Handling Sheet Metal at High Speeds

    Schmalz will provide solutions with a new range of especially adaptable suction pads for extremely dynamic handling of sheet metal and car body parts from mid 2011.

  • 15.10.2010
    Powerful when Handling Glass: SGF Suction Plates

    The new SGF suction plates from Schmalz provide for the best hold on smooth surfaces and reliable and careful handling of flat workpieces, such as glass or plastic sheets, solar modules and collectors.

  • 15.10.2010
    For corners and edges. Vacuum suction pads for dynamic sheet metal handling

    Vacuum specialist Schmalz presents new suction pads for handling structural sheet metal components with round edges and small radii.

  • 12.10.2010
    Efficient Vacuum Generation with Compressed Air

    Pneumatic vacuum ejectors are the best choice for reliable and efficient vacuum generation. Whether you're talking about a basic injector, an inline ejector, a multi-stage ejector, or a compact ejector – the system is not optimally configured until the vacuum generation is matched to the particular application.

  • 15.09.2010
    A Secure Hold in Any Position: Vacuum Suction Pads for Package Handling

    Stable cardboard boxes or flexible-form product packaging – process reliability in dynamic packaging processes goes hand-in-hand with the use of the right suction pad.

  • 30.07.2010
    Holds up its end of the bargain – the new suction pad for flexible-form product packaging

    In automated packaging processes, the gripper used must meet high demands for process reliability and speed. This is especially the case when handling flexible-form packaging with liquid or powdery contents.

  • 29.07.2010
    Innovative Vacuum Handling in Photovoltaic Production

    Wafers, cells, strings, glass, foils and modules – Schmalz offers groundbreaking vacuum handling solutions for the entire photovoltaic production supply chain.

  • 28.07.2010
    Added safety: Mechanical vacuum switches

    Whether they are electro-mechanical or pneumatic, reliable switch elements are the key to safe operation in a vacuum system. Switches that offer added safety are a big plus.

  • 18.03.2010
    Compact Vacuum Generators with IO-Link – Investment with Added Value

    IO-Link technology for vacuum generation using compressed air – with the SCPi/SMPi series, Schmalz is setting technical standards while offering users the benefits of process automation with real added value.

  • 18.03.2010
    Complex Knowledge in Compact Form

    Practical vacuum training set for training centers

  • 14.01.2010
    The perfect grip for sheet metal every time

    Vacuum technology specialist Schmalz provides integrated solutions for the handling of sheet metal and demonstrates expertise right down to the last detail – because only the correct suction pad can hold the workpiece optimally.

Archive
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
Salons

Tous les ans, Schmalz présente ses tout derniers produits sur de nombreux salons.

Plus...